Eaton Logo

iLight series

Where can I download the iLight app?

You can download it for free from the iTunes store of Google Play store. Search for iLight Remote. Read more...

iCANsoft programming guide

Approved users with access to the SW-2 Software Kit can visit the Download Centre where there are programming manuals and other support materials. Read more...

How do I install the driver for the Cooper Controls USB converter?

All the necessary drivers are included with an installation of the iLight software. We recommend that you use latest version of the iLight Read more...

Does iCANsoft work with Windows 10?

Yes, iLight software  (iCANsoft, Device Editor and associated programs) is compatible with Windows 10 if you are using iCANsoft version 3.1.7 or Read more...

iLight Remote app not longer connects to the EG2?

The iLight Remote app works in conjunction with the EG2 Ethernet Gateway. Please ensure that your EG2 is still powered. Cycling the power to the EG2 (turn Read more...

I am looking for a RS232 control commands for iLight

The SC- Wall-mounted Source Controller range support a direct RS485 connection. The RS485 ASCII control commands can be found in the Source Controller Read more...

Can I integrate iLight with Control 4?

Yes, an iLight system can be integrated with Control 4 either using the SI-2 System Integrator for wired RS232 serial connection, or using the EG2 Read more...

looking for sw2 software kit

The SW-2 Software Kit contains the iLight programming software, PC Node CAN interface and connection cables. The SW-2 can be purchased subject to Read more...

My PC Node does not work.

The PC Node is powered from the iLight network so you must first make sure that you have enough voltage at the point where you are connecting your PC Node. Read more...

How to I arrange iLight training?

We run iLight training courses on a by-demand basis from our Watford office (20 Greenhill Crescent, Watford, WD18 8JA). Training is normally spread over Read more...

How do I update my iLight software?

Updates for iLight programming software are available from the Download Centre: www.ilight.info User registration required. Access will be granted Read more...

I am getting an 'unable to open port' message when trying to connect to the iLight network

'Unable to open port' appears when the iLight software is unable to establish a connection with the iLight CAN network. This can be for several Read more...

How do I perform a factory reset for iLight products?

There is no factory reset option, but it is possible to upload a factory default configuration to the device from the iLight software. This can be aquired Read more...

I have a LCD touch panel for my iLight system and the LCD is not working. Can this be replaced?

The TSC30 touchscreen LCD can be replaced. We would require the complete unit to be returned to our service department for repair. To proceed with this, Read more...

What does 'please unlock for device configuration' mean?

This is a request over the network from the iLight software to enable new configuration settings to be applied to an iLight product. If this message Read more...

What is the latest firmware version for the EG2 Ethernet Gateway?

The latest firmware version for the EG2 is 4.05P, and ships with all production devices at this time. If you have a unit with an earlier version it may Read more...

iLight system isn't working, we need someone to help

Please use the Email button on this page to send a support request directly to the technical team. Please explain the problem you are experiencing in as Read more...

Which LED downlights are compatible with SCI type dimmers

The SCI Inductive Source Controller models are leading-edge mains dimming units suitable for controlling resistive and inductive load types. These include Read more...

0-10V lights not turning off completely?

0-10V is distinct from 1-10V in that power does not need to be switched off to achieve zero illumination from the light source. For 0-10V to work, both Read more...

I have forgotten my login details for www.iLight.info

If you have forgotten your password, please choose the 'forgotten password' option on the login screen. If you have forgotten your username, Read more...

Where can I find a list of local sales agents?

Contact details for our UK and International sales agents can be found here:  http://ilight.co.uk/contact.html Contact details for international Read more...

LED

Please be more specific about what aspect of LED lighting you need help with. Read more...

Can I get information on iCANsoft programming and devices configurations in the network

Each device on an iLight system stores its configuration and this can be retrieved by an Eaton Lighting Systems engineer or via iLight programming Read more...

Why after a power failure is touch pad not working?

If a touchscreen is not displaying, the first thing to confirm is whether is power to the unit. The TSC Touchscreen models are powered by a Read more...

Is it possible to turn off the button back light on a Control Panel (keypad)?

To prevent button LEDs on Control Panels from illuminating, set the Select Scene action to the release action of the button, and leave the press Read more...

Supply voltage not supported on device?

Not all iLight products have supply voltage feedback into the software. Control Panels and accessories with the blue connector (previous generation) do Read more...

Are there an iLight specialist service engineer who covers the London area?

Our in-house team of service and commissioning engineers cover the London area. To request a visit, please send details of the matter you need Read more...

Do you sell a motion sensor compatible with iLight systems?

Details about our motion sensors can be found on our main website. Link: http://ilight.co.uk/products-sensors.html Read more...

How do I change iLight touchscreen programming?

An iLight touchscreen configuration is edited using the TSC3050 Editor which is provided as part of the iCANsoft & Tools Suite software package (SW-2 Read more...

What is the purpose of the End-of-Line termination for the iLight CAN bus network?

CAN bus is a high-speed method of data transfer where each differential pair of wires is a transmission line. The end-of-line terminations for the iLight Read more...

Where can I find the manual for the SCi1210S

The Source Controller manual can be found at the iLight website - http://ilight.co.uk/products-source-controllers.html Read more...

I am looking for a London based dealer for iLight

Please call our office on 01923 495495 and ask to speak to Sales. Line open Mon-Fri 9am-5pm. To make sure you're connected to the correct person, Read more...

what is the maximum length of a dali network

The maximum length for a DALI network is 300 meters using 1.5mm2 mains rated 2-core cable. Read more...

What is the factory IP address of an EG2 Ethernet Gateway?

The factory IP address settings for the EG2 Ethernet Gateway are: IP address: 192.168.0.100Subnet mask: 255.255.255.0Gateway: 192.168.0.254 Read more...

What is the recommended cable type for the iCAN network?

The recommended cable type is Belden 1502 Read more...

What is the part number for an SCA1210 output PCB?

The part number is CC0400400 (1 of 3) . The output terminal PCB is part CC0400600 (1 of 3). For pricing, please contact your sales agent or local Read more...

What is the part number for an SCH0410 4x10 contactor PCB?

The part number is CC0401300 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI1205 12x5A output PCB?

The part number is CC0401800 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI0410 processor / CPU PCB?

The part number is CC0400104 . For pricing, please contact your sales agent or local distributor. Read more...

What are the dimensions of an SCMC0410 Din rail Curtain Controller module?

The dimensions (mm) are 90hx160w58d. Read more...

What are the dimensions of an SCS0410 Source Controller?

The dimensions (mm) are 280hx220wx155d for the S version, 340hx255wx155d for the RCBO/RCBOX version and 400hx220wx155d for the D version. Read more...

What are the dimensions of an SCLED0405 Source Controller?

The dimensions (mm) are 280hx220wx155d for the S version, 340hx255wx155d for the RCBO/RCBOX version and 400hx220wx155d for the D version. Read more...

What is the maximum loading for an SCI0405 Inductive Source Controller?

The SCI0405 Inductive Source Controller is rated at 5A per output (1000W @ 240Vac). Please refer to this product's datasheet at www.ilight.co.uk for a Read more...

is there an ilight specialist service engineer for York area

Our iLight Service Engineers cover the whole of the UK. If you would like to book an engineering visit, please email fieldservicecc@eaton.com, or phone 019 Read more...

Remington i-LIGHT IPL 6250

This product is not associated with iLight lighting control systems. Read more...

Extended ASCII PCB

The Extended ASCII PCB is an accessory for most Wall-mounted Source Controller (SC-) types that increases the capabilities of the RS485 in/out port. This Read more...

What is the iCAN network voltage?

The iLight CAN network typically operates at 12-15Vdc. This can be increased up to 18Vdc maximum. Network powered devices such as Control Panels, UIM, UIG2 Read more...

Can I use another processor PCB in my iLight dimmer?

The processor PCB (CPU) in each iLight source controller stores the output settings for that specific unit (Area, Channel, Scene Levels). This information Read more...

What does the Virtual Panel State action mean?

This action works on a 'virtual' level which means that it will be responded to by input devices according to their Area allocation, rather than Read more...

If DALI wires are connected to 240V AC voltage what will happen?

If 240Vac is applied to the DALI control pair this is highly likely to damage the DALI controller and any devices connected to this DALI network (ballasts, Read more...

How many 0-10V / 1-10V drivers can be put on one channel?

0-10V and 1-10V ballast loading varies depending on the type of HF ballast controller being used. This information is provided on the associated datasheet Read more...

Is there a 15V power supply available?

The PSU-15-DIN is a 15Vdc 20W dinrail mounted power supply, 1 module width (17.5mm). The number of devices that can be powered from this power supply will Read more...

Connecting to mains?

Please refer to the product installation manual for details about mains supply connection. IMPORTANT: Installation and termination of mains cabling Read more...

Is it possible to extract the existing project configuration from an iLight system?

Each device connected to the iLight network contains its own configuration data. This can be retrieved from the individual devices via the iLight software Read more...

Can I perform an Earth Loop Impedance test with an iLight system?

When installations are Earth Loop Impedance tested using electronic earth loop impedance testers and the system includes Inductive source controllers (SCI Read more...

How do I set the time/date on a TC-1 Timeclock?

To adjust the time/date/day of the week for a TC-1 Astronomical Timeclock: From the main screen press 1 on the keypad then choose from the following Read more...

I am looking for a EM6784

EM6784 is the 12 x 5A output PCB for the SCi1205 Source Controller. Order code is CC04-018-00 If you would like to order this part please send your Read more...

How do you copy a sequence to another device?

In the Sequences tab, go to the relevant sequence and right-click on any of the action lines of the sequence, then choose Select All. Right-click again an Read more...

How do I update the firmware in an NS3-C Network Sensor?

The iLight NS3-C Network Sensor is updated over the iLight network via iLight programming software, using the Flash Tool utility. IMPORTANT Firmware Read more...

Can a 1-10v dimming luminaire be incorporated into a DALI control system?

Eaton Lighting Systems tdo not currently offer DALI-1-10V converters. However, there are some available on the market. Read more...

TSC3050 Touchscreen Editor upload error "The application has failed to start because its side by side configuration is incorrect".

This error occurs if Windows is trying to run an incorrect version of the C++ Runtime Libraries which are utilised by many programs. This may be Read more...

Touchscreen not working

Please click on the Email button below to open a ticket and an engineer will be able to assist you. Please the following information: Site name/ Read more...

How do you install a di-1 dmx input PCB to a source controller?

The DI-1 DMX Input card plugs into the 10-pin socket on the Source Controller CPU card. The Source Controller’s power must be reset after Read more...

What are dimensions for the TSC30 / TSX30 back box?

The TSC30 & TSX30 fit into a UK standard double-gang wall box (146mm x 86mm) with minimum depth of 35mm. NOTE: Wall box not supplied with the TSC3 Read more...

SCLED

Please type a more specific question to help us find the right answer for you regarding the SCLED. For datasheets and installation guides on this product, Read more...

What is the maximum delay time for a sequence action?

Max sequence delay is 56m 36.75s per line/action Read more...

How do I override an iLight Source Controller?

For wall mounted Source Controllers: Press and hold the button to the left of the green status LED on the underside of the Source Controller.  After Read more...

What is the maximum number of devices that can be connected to an iCAN network?

A maximum of 100 devices (all types) can be connected to a single iCAN network. This can be increased using the BN-2 Network Bridge / Repeater module. Read more...

What is the maximum distance of an iCAN network?

The iCAN network should not exceed 500m in length, but this can be increased using the BN-2 Network Bridge / Repeater module. Read more...

What is the part number for a TC-1 Timeclock PCB?

The part number is CC0404000 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an RI-2 Relay Interface PCB?

The part number is CC0405500 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCD96 DMX Source Controller PCB?

The part number is CC0405600 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCD24 DMX Source Controller DMX Output PCB?

The part number is CC0498000 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCD24 DMX Source Controller processor PCB?

The part number is CC0400115 . The processor must be fitted with the DMX Output PCB - part CC0498000 - for correct operation. For pricing, please contact Read more...

What is the part number for an SCH1210/SCH1220 HF output PCB?

The part number is CC0404800 (HF card only). The HF card & 12-channel contactor PCB can be ordered as an assembled set as CC0400900. For pricing, please Read more...

What is the part number for an SCI0805 8x5A output PCB?

The part number is CC0401200 (-S, -T and -TN version) or CC0403000 (-N version) . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCS1220 output PCB?

The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCS1210 output PCB?

The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCS0420 output PCB?

The part number is CC0404400 (-S & -RCBO/RCBOX versions) or CC0404500 (-N or -D versions) For pricing, please contact your sales agent or local Read more...

What is the part number for an SCS0410 output PCB?

The part number is CC0404400 (-S & -RCBO/RCBOX versions) or CC0404500 (-N or -D versions) For pricing, please contact your sales agent or local Read more...

What is the part number for an SCA0410 4x10A output PCB?

The part number is CC0400400 . The output terminal PCB is part CC0400600. For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCH1220 12x20A contactor PCB?

The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCH1210 12x10A contactor PCB?

The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCLED1205 12x5A output PCB?

The part number is CC0406001 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCLED0405 4x5A output PCB?

The part number is CC0406101 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI1220 output PCB?

The part number is CC0401500 (1 of 3) . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI1210 output PCB?

The part number is CC0401500 (1 of 3) . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI0420 4x20A output PCB?

The part number is CC0401500 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI0410 4x10A output PCB?

The part number is CC0401600 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI0405 4x5A output PCB?

The part number is CC0401400 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCI0805 processor / CPU PCB?

The part number is CC0400105 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCS1220 processor / CPU PCB?

The part number is CC0400110 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCS1210 processor / CPU PCB?

The part number is CC0400110 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCS0410 processor / CPU PCB?

The part number is CC0400109 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCA1210 processor / CPU PCB?

The part number is CC0400108 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCA0410 processor / CPU PCB?

The part number is CC0400107 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCH1220 processor / CPU PCB?

The part number is CC0400114 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCH1210 processor / CPU PCB?

The part number is CC0400114 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCH0410 processor / CPU PCB?

The part number is CC0400111 . For pricing, please contact your sales agent or local distributor. Read more...

What is the part number for an SCLED1205 processor / CPU PCB?

The part number is CC0400118 . For pricing, please contact your sales agent or local distributor. Read more...