iLight Hardware
What is the iCAN network voltage?
The iLight CAN network typically operates at 12-15Vdc. This can be increased up to 18Vdc maximum. Network powered devices such as Control Panels, UIM, UIG2 Read more...
iLight Remote app not longer connects to the EG2?
The iLight Remote app works in conjunction with the EG2 Ethernet Gateway. Please ensure that your EG2 is still powered. Cycling the power to the EG2 (turn Read more...
Can I integrate iLight with Control 4?
Yes, an iLight system can be integrated with Control 4 either using the SI-2 System Integrator for wired RS232 serial connection, or using the EG2 Read more...
If DALI wires are connected to 240V AC voltage what will happen?
If 240Vac is applied to the DALI control pair this is highly likely to damage the DALI controller and any devices connected to this DALI network (ballasts, Read more...
Extended ASCII PCB
The Extended ASCII PCB is an accessory for most Wall-mounted Source Controller (SC-) types that increases the capabilities of the RS485 in/out port. This Read more...
Can I use another processor PCB in my iLight dimmer?
The processor PCB (CPU) in each iLight source controller stores the output settings for that specific unit (Area, Channel, Scene Levels). This information Read more...
0-10V lights not turning off completely?
0-10V is distinct from 1-10V in that power does not need to be switched off to achieve zero illumination from the light source. For 0-10V to work, both Read more...
Do you sell a motion sensor compatible with iLight systems?
Details about our motion sensors can be found on our main website. Link: http://ilight.co.uk/products-sensors.html Read more...
How do you install a di-1 dmx input PCB to a source controller?
The DI-1 DMX Input card plugs into the 10-pin socket on the Source Controller CPU card. The Source Controller’s power must be reset after Read more...
SCLED
Please type a more specific question to help us find the right answer for you regarding the SCLED. For datasheets and installation guides on this product, Read more...
What is the part number for an SCLED1205 12x5A output PCB?
The part number is CC0406001 . For pricing, please contact your sales agent or local distributor. Read more...
What are the dimensions of an SCLED1205 Source Controller?
The dimensions (mm) are 550hx220wx155d for the S version, 550hx255wx155d for the RCBO/RCBOX version and 690hx220wx155d for the D version. Read more...
What routine maintenance checks are carried out?
Standard Maintenance Checks: · Read all the devices in and make sure they are all responding. Read more...
Why after a power failure is touch pad not working?
If a touchscreen is not displaying, the first thing to confirm is whether is power to the unit. The TSC Touchscreen models are powered by a Read more...
Supply voltage not supported on device?
Not all iLight products have supply voltage feedback into the software. Control Panels and accessories with the blue connector (previous generation) do Read more...
Connecting to mains?
Please refer to the product installation manual for details about mains supply connection. IMPORTANT: Installation and termination of mains cabling Read more...
How do I perform a factory reset for iLight products?
There is no factory reset option, but it is possible to upload a factory default configuration to the device from the iLight software. This can be aquired Read more...
What does 'please unlock for device configuration' mean?
This is a request over the network from the iLight software to enable new configuration settings to be applied to an iLight product. If this message Read more...
Where can I find the manual for the SCi1210S
The Source Controller manual can be found at the iLight website - http://ilight.co.uk/products-source-controllers.html Read more...
What is the latest firmware version for the EG2 Ethernet Gateway?
The latest firmware version for the EG2 is 4.05P, and ships with all production devices at this time. If you have a unit with an earlier version it may Read more...
What are dimensions for the TSC30 / TSX30 back box?
The TSC30 & TSX30 fit into a UK standard double-gang wall box (146mm x 86mm) with minimum depth of 35mm. NOTE: Wall box not supplied with the TSC3 Read more...
What is the part number for an SCS0410 output PCB?
The part number is CC0404400 (-S & -RCBO/RCBOX versions) or CC0404500 (-N or -D versions) For pricing, please contact your sales agent or local Read more...
What is the part number for an SCA0410 4x10A output PCB?
The part number is CC0400400 . The output terminal PCB is part CC0400600. For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCLED0405 4x5A output PCB?
The part number is CC0406101 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI0410 4x10A output PCB?
The part number is CC0401600 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCS1220 processor / CPU PCB?
The part number is CC0400110 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCLED1205 processor / CPU PCB?
The part number is CC0400118 . For pricing, please contact your sales agent or local distributor. Read more...
Can I control an iLight Source Controller with DMX?
Most Source Controller types can be converted to allow control by a DMX input with the addition of the DI-1 DMX Input PCB. Please consult the Source Read more...
What is the maximum loading for an SCMA0402 Adaptive Din rail module?
Outputs are individually rated for 2.5A with a maximum module loading of 10A. Consult the product datasheet for more information or contact Technical Read more...
What are the dimensions of an SCD96 DMX Controller?
The dimensions (mm) are 240hx220wx80d. Read more...
What are the dimensions of an SCMS0810 Din rail Switched module?
The dimensions (mm) are 90hx160w58d. Read more...
Can an iLight system be used to control motorised blinds and curtains?
Yes. Motorised blinds and curtains can be controlled using either the wall-mounted RI-2 Relay Interface or the Din rail mounted SCMC0410 module (MPM2400 Read more...
What are the dimensions of an SCA1210 Source Controller?
The dimensions (mm) are 850hx330wx155d. The RCBO/RCBOX version please contact Technical Support. Read more...
What is the maximum loading for an SCA1210 Adaptive Source Controller?
The SCA1210 Adaptive Source Controller is rated at 10A per output (1000W @ 240Vac). NOTE: Derating to 10% maximum load is recommended for most LED load Read more...
What is the maximum loading for an SCH1210 HF Ballast Source Controller?
The SCH1210 HF Ballast Source Controller is rated at 10A per output (2000W @ 240Vac). Please refer to this product's datasheet at www.ilight.co.uk for a Read more...
What is the maximum loading for an SCI1210 Inductive Source Controller?
The SCI1210 Inductive Source Controller is rated at 10A per output (2000W @ 240Vac). Please refer to this product's datasheet at www.ilight.co.uk for a Read more...
I have a LCD touch panel for my iLight system and the LCD is not working. Can this be replaced?
The TSC30 touchscreen LCD can be replaced. We would require the complete unit to be returned to our service department for repair. To proceed with this, Read more...
What does the Virtual Panel State action mean?
This action works on a 'virtual' level which means that it will be responded to by input devices according to their Area allocation, rather than Read more...
Which LED downlights are compatible with SCI type dimmers
The SCI Inductive Source Controller models are leading-edge mains dimming units suitable for controlling resistive and inductive load types. These include Read more...
How many 0-10V / 1-10V drivers can be put on one channel?
0-10V and 1-10V ballast loading varies depending on the type of HF ballast controller being used. This information is provided on the associated datasheet Read more...
Is there a 15V power supply available?
The PSU-15-DIN is a 15Vdc 20W dinrail mounted power supply, 1 module width (17.5mm). The number of devices that can be powered from this power supply will Read more...
Can I perform an Earth Loop Impedance test with an iLight system?
When installations are Earth Loop Impedance tested using electronic earth loop impedance testers and the system includes Inductive source controllers (SCI Read more...
How do I set the time/date on a TC-1 Timeclock?
To adjust the time/date/day of the week for a TC-1 Astronomical Timeclock: From the main screen press 1 on the keypad then choose from the following Read more...
I am looking for a EM6784
EM6784 is the 12 x 5A output PCB for the SCi1205 Source Controller. Order code is CC04-018-00 If you would like to order this part please send your Read more...
What is the purpose of the End-of-Line termination for the iLight CAN bus network?
CAN bus is a high-speed method of data transfer where each differential pair of wires is a transmission line. The end-of-line terminations for the iLight Read more...
Touchscreen not working
Please click on the Email button below to open a ticket and an engineer will be able to assist you. Please the following information: Site name/ Read more...
How do I override an iLight Source Controller?
For wall mounted Source Controllers: Press and hold the button to the left of the green status LED on the underside of the Source Controller. After Read more...
What is the part number for a TC-1 Timeclock PCB?
The part number is CC0404000 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an RI-2 Relay Interface PCB?
The part number is CC0405500 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCD96 DMX Source Controller PCB?
The part number is CC0405600 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCD24 DMX Source Controller DMX Output PCB?
The part number is CC0498000 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCD24 DMX Source Controller processor PCB?
The part number is CC0400115 . The processor must be fitted with the DMX Output PCB - part CC0498000 - for correct operation. For pricing, please contact Read more...
What is the part number for an SCH1210/SCH1220 HF output PCB?
The part number is CC0404800 (HF card only). The HF card & 12-channel contactor PCB can be ordered as an assembled set as CC0400900. For pricing, please Read more...
What is the part number for an SCI0805 8x5A output PCB?
The part number is CC0401200 (-S, -T and -TN version) or CC0403000 (-N version) . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCS1220 output PCB?
The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCS1210 output PCB?
The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCS0420 output PCB?
The part number is CC0404400 (-S & -RCBO/RCBOX versions) or CC0404500 (-N or -D versions) For pricing, please contact your sales agent or local Read more...
What is the part number for an SCA1210 output PCB?
The part number is CC0400400 (1 of 3) . The output terminal PCB is part CC0400600 (1 of 3). For pricing, please contact your sales agent or local Read more...
What is the part number for an SCH1220 12x20A contactor PCB?
The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCH1210 12x10A contactor PCB?
The part number is CC0401700 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCH0410 4x10 contactor PCB?
The part number is CC0401300 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI1220 output PCB?
The part number is CC0401500 (1 of 3) . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI1210 output PCB?
The part number is CC0401500 (1 of 3) . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI1205 12x5A output PCB?
The part number is CC0401800 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI0420 4x20A output PCB?
The part number is CC0401500 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI0405 4x5A output PCB?
The part number is CC0401400 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI0805 processor / CPU PCB?
The part number is CC0400105 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCS1210 processor / CPU PCB?
The part number is CC0400110 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCS0410 processor / CPU PCB?
The part number is CC0400109 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCA1210 processor / CPU PCB?
The part number is CC0400108 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCA0410 processor / CPU PCB?
The part number is CC0400107 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCH1220 processor / CPU PCB?
The part number is CC0400114 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCH1210 processor / CPU PCB?
The part number is CC0400114 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCH0410 processor / CPU PCB?
The part number is CC0400111 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCLED0405 processor / CPU PCB?
The part number is CC0400117 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI1220 processor / CPU PCB?
The part number is CC0400201 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI1210 processor / CPU PCB?
The part number is CC0400201 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI1205 processor / CPU PCB?
The part number is CC0400106 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI0420 processor / CPU PCB?
The part number is CC0400104 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI0410 processor / CPU PCB?
The part number is CC0400104 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for an SCI0405 processor / CPU PCB?
The part number is CC0400104 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for a UIG-2 Universal Interface PCB?
The part number is CC0405700 . For pricing, please contact your sales agent or local distributor. Read more...
What is the part number for Classic Control Panel PCB?
The 9-button PCB with programming socket is part number CC0403600. A 9-button PCB with IR receiver is part number CC0403700. A 10-button PCB is part Read more...
What do the green and red LED underneath a Source Controller indicate?
The green status LED indicates the status of the processor PCB. It should be flashing once every second under normal operation. If it is not illuminated Read more...
Which iLight Source Controllers are compatible with trailing-edge dimming mains dimming?
The SCLED Transistor and SCA Adaptive Source Controller types can be configured to run in trailing-edge mode (by output). The SCMA0402 Apative Din rail Read more...
Which iLight Source Controllers are compatible with leading-edge dimming mains dimming?
The SCI Inductive type Source Controllers and SCMI Inductive Din rail module are for leading-edge mains dimming. The SCLED Transistor and SCA Adaptive Read more...
What is the maximum loading for an SCMC0410 Din rail Curtain Controller module?
Outputs are individually rated for 10A with a maximum module loading of 40A. Consult the product datasheet for more information or contact Technical Read more...
What is the maximum loading for an SCMR0816 Switched Relay Din rail module?
Outputs are individually rated for 16A. Consult the product datasheet for more information or contact Technical Support with any specific loading Read more...
What is the maximum loading for an SCS0810 Switched Din rail module?
Outputs are individually rated for 10A with a maximum module loading of 16A. Consult the product datasheet for more information or contact Technical Read more...
What is the maximum loading for an SCS0410 Switched Din rail module?
Outputs are individually rated for 10A with a maximum module loading of 16A. Consult the product datasheet for more information or contact Technical Read more...
What is the maximum loading for an SCH0410 Inductive Source Controller?
Outputs are individually rated for 10A with a maximum module loading of 16A. Consult the product datasheet for more information or contact Technical Read more...
What is the maximum loading for an SCMI0402 Inductive Din rail module?
Outputs are individually rated for 10A with a maximum module loading of 16A. Consult the product datasheet for more information or contact Technical Read more...
What is the maximum number of modules that can be connected to an MPM2400 Din rail Master Processor?
The maximum number of outputs that an MPM2400 can control is 24, so the quantity of Din rail modules is dependent on their total number of outputs (some Read more...
What are the dimensions of an SCMD6400 Din rail Addressable DALi Controller?
The dimensions (mm) are 90hx160w58d. NOTE: This unit does not require connection to an MPM2400 Master Processor Read more...
What are the dimensions of an SCMA0402 Din rail Adaptive module?
The dimensions (mm) are 90hx227w48d. NOTE: This unit does not require connection to an MPM2400 Master Processor. Read more...
What are the dimensions of an SCMR0816 Din rail Switched module?
The dimensions (mm) are 90hx160w58d. Read more...
What are the dimensions of an SCMC0410 Din rail Curtain Controller module?
The dimensions (mm) are 90hx160w58d. Read more...
What are the dimensions of an SCMS0410 Din rail Switched module?
The dimensions (mm) are 90hx160w58d. Read more...
What are the dimensions of an SCMH0410 Din rail HF Ballast module?
The dimensions (mm) are 90hx160w58d. Read more...
What are the dimensions of an SCMI0402 Din rail Inductive module?
The dimensions (mm) are 90hx160w58d. Read more...