Eaton Logo

Which iLight Source Controllers are compatible with leading-edge dimming mains dimming?

The SCI Inductive type Source Controllers and SCMI Inductive Din rail module are for leading-edge mains dimming. The SCLED Transistor and SCA Adaptive Source Controller types can be configured to run in leading-edge mode (by output). The SCMA0402 Apative Din rail module will auto-select leading or trailing-edge dimming mode according to the load type detected.