Eaton Logo

How do I override an iLight Source Controller?

For wall mounted Source Controllers:

  1. Press and hold the button to the left of the green status LED on the underside of the Source Controller.
     
  2. After approx. 10 seconds the green and red status LED on the underside of the Source Controller will start to flash together. The unit is now in override mode.
     
  3. Release the button and then press it again once (momentarily). The green status LED will turn off and all outputs on the Source Controller will be energised to full power (100%).
     
  4. A seconds press of this same button will turn all outputs off (0%).
     
  5. A third press of this same button will make the green and red status LEDs start to flash together. At this point you can choose the following options:

a) Press and hold this same button for approx. 10 seconds to exit override mode and return to normal operation. The last select scene for each Area will be recalled.

b) Press the button once (momentarily) to return to step 3.

 

For Din rail Modules:

  1. Press and hold the Ident button on an MPM Master Processor to override all connected output modules, or press and hold the Ident button on a specific output module to only override those outputs.
     
  2. After approx. 10 seconds the green and red status LED on the module will start to flash together. The module is now in override mode.
     
  3. Release the button and then press it again once (momentarily). The green status LED will turn off and all outputs on the module(s) will be energised to full power (100%).
     
  4. A seconds press of this same button will turn all outputs off (0%).
     
  5. A third press of this same button will make the green and red status LEDs start to flash together. At this point you can choose the following options:

a) Press and hold this same button for approx. 10 seconds to exit override mode and return to normal operation. The last select scene for each Area will be recalled.

b) Press the button once (momentarily) to return to step 3.