Accessories
iLight Remote app not longer connects to the EG2?
The iLight Remote app works in conjunction with the EG2 Ethernet Gateway. Please ensure that your EG2 is still powered. Cycling the power to the EG2 (turn Read more...
My PC Node does not work.
The PC Node is powered from the iLight network so you must first make sure that you have enough voltage at the point where you are connecting your PC Node. Read more...
I have a LCD touch panel for my iLight system and the LCD is not working. Can this be replaced?
The TSC30 touchscreen LCD can be replaced. We would require the complete unit to be returned to our service department for repair. To proceed with this, Read more...
How do I set the time/date on a TC-1 Timeclock?
To adjust the time/date/day of the week for a TC-1 Astronomical Timeclock: From the main screen press 1 on the keypad then choose from the following Read more...
Extended ASCII PCB
The Extended ASCII PCB is an accessory for most Wall-mounted Source Controller (SC-) types that increases the capabilities of the RS485 in/out port. This Read more...
Is there a 15V power supply available?
The PSU-15-DIN is a 15Vdc 20W dinrail mounted power supply, 1 module width (17.5mm). The number of devices that can be powered from this power supply will Read more...
Can a 1-10v dimming luminaire be incorporated into a DALI control system?
Eaton Lighting Systems tdo not currently offer DALI-1-10V converters. However, there are some available on the market. Read more...