Eaton Logo

Control Panels

What is the iCAN network voltage?

The iLight CAN network typically operates at 12-15Vdc. This can be increased up to 18Vdc maximum. Network powered devices such as Control Panels, UIM, UIG2 Read more...

I have a LCD touch panel for my iLight system and the LCD is not working. Can this be replaced?

The TSC30 touchscreen LCD can be replaced. We would require the complete unit to be returned to our service department for repair. To proceed with this, Read more...

Is it possible to turn off the button back light on a Control Panel (keypad)?

To prevent button LEDs on Control Panels from illuminating, set the Select Scene action to the release action of the button, and leave the press Read more...

What does the Virtual Panel State action mean?

This action works on a 'virtual' level which means that it will be responded to by input devices according to their Area allocation, rather than Read more...

What are dimensions for the TSC30 / TSX30 back box?

The TSC30 & TSX30 fit into a UK standard double-gang wall box (146mm x 86mm) with minimum depth of 35mm. NOTE: Wall box not supplied with the TSC3 Read more...

Supply voltage not supported on device?

Not all iLight products have supply voltage feedback into the software. Control Panels and accessories with the blue connector (previous generation) do Read more...

Touchscreen not working

Please click on the Email button below to open a ticket and an engineer will be able to assist you. Please the following information: Site name/ Read more...

Why after a power failure is touch pad not working?

If a touchscreen is not displaying, the first thing to confirm is whether is power to the unit. The TSC Touchscreen models are powered by a Read more...