Sensors & Interfaces
Do you sell a motion sensor compatible with iLight systems?
Details about our motion sensors can be found on our main website. Link: http://ilight.co.uk/products-sensors.html Read more...
What is the latest firmware version for the EG2 Ethernet Gateway?
The latest firmware version for the EG2 is 4.05P, and ships with all production devices at this time. If you have a unit with an earlier version it may Read more...
I am looking for a RS232 control commands for iLight
The SC- Wall-mounted Source Controller range support a direct RS485 connection. The RS485 ASCII control commands can be found in the Source Controller Read more...
What is the iCAN network voltage?
The iLight CAN network typically operates at 12-15Vdc. This can be increased up to 18Vdc maximum. Network powered devices such as Control Panels, UIM, UIG2 Read more...
My PC Node does not work.
The PC Node is powered from the iLight network so you must first make sure that you have enough voltage at the point where you are connecting your PC Node. Read more...
How do I update the firmware in an NS3-C Network Sensor?
The iLight NS3-C Network Sensor is updated over the iLight network via iLight programming software, using the Flash Tool utility. IMPORTANT Firmware Read more...
What does the Virtual Panel State action mean?
This action works on a 'virtual' level which means that it will be responded to by input devices according to their Area allocation, rather than Read more...
Can I integrate iLight with Control 4?
Yes, an iLight system can be integrated with Control 4 either using the SI-2 System Integrator for wired RS232 serial connection, or using the EG2 Read more...
What are the dimensions of an RI-2 Relay Interface?
The dimensions (mm) are 240hx220wx80d. Read more...
What is the maximum quantity of motorised blinds / curtains that can be connected to an RI-2 Relay Interface?
The RI-2 Relay Interface has 8 x 3A change-over relay outputs available, but maximum quantity of motors that can be connected will vary acccording to the Read more...