Eaton Logo

What is the iCAN network voltage?

The iLight CAN network typically operates at 12-15Vdc. This can be increased up to 18Vdc maximum. Network powered devices such as Control Panels, UIM, UIG2 and BN-2, will require a minimum of 9.5Vdc to operate, but network design should be based upon providing 12Vdc to all devices.

Additional power supplies are available to boost network voltage and should be installed where the voltage is low to lift it to within the acceptable range.